StandardViewsBuilderType Enumeration¶
NXOpen.Drawings.StandardViewsBuilder.Type is an alias for NXOpen.Drawings.StandardViewsBuilderType
-
class
NXOpen.Drawings.
StandardViewsBuilderType
¶ Bases:
object
The view Layout type
Enum Members
Enum Member Enum Member Description FrontTop front, top FrontRight front, right FrontLeft front, left FrontTopRight front, top, right FrontTopLeft front, top, left FrontTopRightIso front, top, right, iso FrontTopLeftIso front, top, left, iso -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-