ShipDraftingViewLinesViewStyleLines Enumeration¶
NXOpen.Drawings.ShipDraftingViewLinesViewStyle.Lines is an alias for NXOpen.Drawings.ShipDraftingViewLinesViewStyleLines
-
class
NXOpen.Drawings.
ShipDraftingViewLinesViewStyleLines
¶ Bases:
object
Line type
Enum Members
Enum Member Enum Member Description HiddenNonsection Hidden, NonSection VisibleNonsection Visible, NonSection HiddenSection Hidden, Section VisibleSection Visible, Section SecondaryHiddenNonsection Secondary, Hidden, NonSection SecondaryVisibleNonsection Secondary, Visible, NonSection SecondaryHiddenSection Secondary, Hidden, Section SecondaryVisibleSection Secondary, Visible, Section -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-