SectionLineSegmentsBuilder Class¶
-
class
NXOpen.Drawings.
SectionLineSegmentsBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a class Drawings.
SectionLineSegmentsBuilder.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
RotationPoint | Returns or sets the rotation point |
SectionLineOnlyPlacementOrigin | Returns or sets the section line only placement origin center in inferred mode |
SegmentLocation | Returns the segment location |
SegmentLocationForSecondLeg | Returns the segment location to add segments to revolved section line second leg |
SingleLeg | Returns or sets the single leg |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
UpdateAfterParentViewMove | Update the section line segments builder in case of parent view move |
Property Detail¶
RotationPoint¶
-
SectionLineSegmentsBuilder.
RotationPoint
¶ Returns or sets the rotation point
-------------------------------------
Getter Method
Signature
RotationPoint
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationPoint
Parameters: rotationPointTag ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: None.
SectionLineOnlyPlacementOrigin¶
-
SectionLineSegmentsBuilder.
SectionLineOnlyPlacementOrigin
¶ Returns or sets the section line only placement origin center in inferred mode
-------------------------------------
Getter Method
Signature
SectionLineOnlyPlacementOrigin
Returns: Return type: NXOpen.Point3d
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionLineOnlyPlacementOrigin
Parameters: coordinates ( NXOpen.Point3d
) –New in version NX10.0.0.
License requirements: None.
SegmentLocation¶
-
SectionLineSegmentsBuilder.
SegmentLocation
¶ Returns the segment location
-------------------------------------
Getter Method
Signature
SegmentLocation
Returns: Return type: NXOpen.Drawings.SectionLineSegmentPointListBuilder
New in version NX10.0.0.
License requirements: None.
SegmentLocationForSecondLeg¶
-
SectionLineSegmentsBuilder.
SegmentLocationForSecondLeg
¶ Returns the segment location to add segments to revolved section line second leg
-------------------------------------
Getter Method
Signature
SegmentLocationForSecondLeg
Returns: Return type: NXOpen.Drawings.SectionLineSegmentPointListBuilder
New in version NX10.0.0.
License requirements: None.
SingleLeg¶
-
SectionLineSegmentsBuilder.
SingleLeg
¶ Returns or sets the single leg
-------------------------------------
Getter Method
Signature
SingleLeg
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SingleLeg
Parameters: singleLeg (bool) – New in version NX10.0.0.
License requirements: None.