SectionLineSegmentPointBuilderSegmentTypes Enumeration

NXOpen.Drawings.SectionLineSegmentPointBuilder.SegmentTypes is an alias for NXOpen.Drawings.SectionLineSegmentPointBuilderSegmentTypes

class NXOpen.Drawings.SectionLineSegmentPointBuilderSegmentTypes

Bases: object

Section Segment Types

Enum Members

Enum Member Enum Member Description
Arrow
Cut
Bend
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.