SectionLineSegmentBuilderTypes Enumeration¶
NXOpen.Drawings.SectionLineSegmentBuilder.Types is an alias for NXOpen.Drawings.SectionLineSegmentBuilderTypes
-
class
NXOpen.Drawings.
SectionLineSegmentBuilderTypes
¶ Bases:
object
the point
Enum Members
Enum Member Enum Member Description Angle Section line cut segment used by: NXOpen.Drawings.PointAndAngleSectionLineBuilder
.Cut Section line cut segment used by: NXOpen.Drawings.PointToPointSectionLineBuilder
NXOpen.Drawings.RevolvedSectionLineBuilder
NXOpen.Drawings.SteppedSectionLineBuilder
Bend Section line bend segment used by: NXOpen.Drawings.PointToPointSectionLineBuilder
NXOpen.Drawings.RevolvedSectionLineBuilder
NXOpen.Drawings.SteppedSectionLineBuilder
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-