SectionLineCollection Class¶
Methods¶
Method | Description |
---|---|
CreateSectionLineBuilder | Creates the section line builder |
CreateSectionLineSegmentBuilder | Creates the section line segment builder |
CreateSectionLineStyleBuilder | Creates the Section Line Style Builder |
CreateSketchSectionLineBuilder | Creates the Sketch Section Line builder |
GenerateSectionLineLabelAttribute | Generates a parametric text attribute that is similar to the current section line label but contains the section line segment information. |
Method Detail¶
CreateSectionLineBuilder¶
-
SectionLineCollection.
CreateSectionLineBuilder
¶ Creates the section line builder
Signature
CreateSectionLineBuilder(sectionLine)
Parameters: sectionLine ( NXOpen.Drawings.SectionLine
) –Returns: Return type: NXOpen.Drawings.SectionLineBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionLineSegments()
instead.License requirements: drafting (“DRAFTING”)
CreateSectionLineSegmentBuilder¶
-
SectionLineCollection.
CreateSectionLineSegmentBuilder
¶ Creates the section line segment builder
Signature
CreateSectionLineSegmentBuilder()
Returns: Return type: NXOpen.Drawings.SectionLineSegmentBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionLineSegments()
instead.License requirements: drafting (“DRAFTING”)
CreateSectionLineStyleBuilder¶
-
SectionLineCollection.
CreateSectionLineStyleBuilder
¶ Creates the Section Line Style Builder
Signature
CreateSectionLineStyleBuilder(sectionline)
Parameters: sectionline ( NXOpen.Drawings.SectionLine
) –Returns: Return type: NXOpen.Drawings.SectionLineStyleBuilder
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder
instead.License requirements: drafting (“DRAFTING”)
CreateSketchSectionLineBuilder¶
-
SectionLineCollection.
CreateSketchSectionLineBuilder
¶ Creates the Sketch Section Line builder
Signature
CreateSketchSectionLineBuilder(sectionLine)
Parameters: sectionLine ( NXOpen.Drawings.SectionLine
) –Returns: Return type: NXOpen.Drawings.SketchSectionLineBuilder
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
GenerateSectionLineLabelAttribute¶
-
SectionLineCollection.
GenerateSectionLineLabelAttribute
¶ Generates a parametric text attribute that is similar to the current section line label but contains the section line segment information.
Note that the text in the section line note is not overwritten.
Signature
GenerateSectionLineLabelAttribute(note)
Parameters: note ( NXOpen.Annotations.BaseNote
) – The section line note to generate the attribute fromReturns: Return type: str New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)