SectionLineBuilderTypes Enumeration¶
NXOpen.Drawings.SectionLineBuilder.Types is an alias for NXOpen.Drawings.SectionLineBuilderTypes
-
class
NXOpen.Drawings.
SectionLineBuilderTypes
¶ Bases:
object
Section Line type
Enum Members
Enum Member Enum Member Description SimpleOrStepped Creates or edits a NXOpen.Drawings.SteppedSectionLine
Half Creates or edits a NXOpen.Drawings.HalfSectionLine
Revolved Creates or edits a NXOpen.Drawings.RevolvedSectionLine
PointToPoint Creates or edits a NXOpen.Drawings.PointToPointSectionLine
PointAndAngle Creates or edits a NXOpen.Drawings.PointAndAngleSectionLine
Pictorial Creates or edits a NXOpen.Drawings.PictorialSectionLine
HalfPictorial Creates or edits a NXOpen.Drawings.HalfPictorialSectionLine
Oriented Creates or edits a NXOpen.Drawings.OrientedSectionLine
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-