ScalePositionTypes Enumeration

class NXOpen.Drawings.ScalePositionTypes

Bases: object

scale Position type Enum Members

Enum Member Enum Member Description
Above
Below
Before
After
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.