MarkAsTemplateBuilderTemplateTypeEnum Enumeration

NXOpen.Drawings.MarkAsTemplateBuilder.TemplateTypeEnum is an alias for NXOpen.Drawings.MarkAsTemplateBuilderTemplateTypeEnum

class NXOpen.Drawings.MarkAsTemplateBuilderTemplateTypeEnum

Bases: object

the template type enum.

Enum Members

Enum Member Enum Member Description
Sheet
ReferenceExistingPart
Standalone
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.