MarkAsTemplateBuilderRelationTypeEnum Enumeration

NXOpen.Drawings.MarkAsTemplateBuilder.RelationTypeEnum is an alias for NXOpen.Drawings.MarkAsTemplateBuilderRelationTypeEnum

class NXOpen.Drawings.MarkAsTemplateBuilderRelationTypeEnum

Bases: object

the relation type enum.

Enum Members

Enum Member Enum Member Description
Master
Specification
Manifestation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.