MarkAsTemplateBuilderItemTypeEnum Enumeration

NXOpen.Drawings.MarkAsTemplateBuilder.ItemTypeEnum is an alias for NXOpen.Drawings.MarkAsTemplateBuilderItemTypeEnum

class NXOpen.Drawings.MarkAsTemplateBuilderItemTypeEnum

Bases: object

the item type enum.

Enum Members

Enum Member Enum Member Description
Any
NXPart
NXDrawing
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.