MarkAsTemplateBuilderActionTypeEnum Enumeration

NXOpen.Drawings.MarkAsTemplateBuilder.ActionTypeEnum is an alias for NXOpen.Drawings.MarkAsTemplateBuilderActionTypeEnum

class NXOpen.Drawings.MarkAsTemplateBuilderActionTypeEnum

Bases: object

the action type enum.

Enum Members

Enum Member Enum Member Description
TemplateOnly
TemplateAndPax
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.