HingeLineBuilderHingeline Enumeration¶
NXOpen.Drawings.HingeLineBuilder.Hingeline is an alias for NXOpen.Drawings.HingeLineBuilderHingeline
-
class
NXOpen.Drawings.
HingeLineBuilderHingeline
¶ Bases:
object
Specifies the hinge line vector option
Enum Members
Enum Member Enum Member Description Inferred The option to infer a hinge line based on parent, child view position Defined The option for selecting hinge line using vector construction tools -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-