HalfSectionLineBuilder Class¶
-
class
NXOpen.Drawings.
HalfSectionLineBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Drawings.HalfSectionLineBuilder
.This class is used to create or edit a
NXOpen.Drawings.HalfSectionLine
. .. versionadded:: NX6.0.0Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionViewType()
instead.
Properties¶
Property | Description |
---|---|
BendLocation | Returns or sets the bend location |
CutLocation | Returns or sets the cut location |
EndLocation1 | Returns or sets the arrow location |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BendLocation¶
-
HalfSectionLineBuilder.
BendLocation
¶ Returns or sets the bend location
-------------------------------------
Getter Method
Signature
BendLocation
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionLineSegments()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
BendLocation
Parameters: bendLocation ( NXOpen.Point
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionLineSegments()
instead.License requirements: drafting (“DRAFTING”)
CutLocation¶
-
HalfSectionLineBuilder.
CutLocation
¶ Returns or sets the cut location
-------------------------------------
Getter Method
Signature
CutLocation
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionLineSegments()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
CutLocation
Parameters: cutLocation ( NXOpen.Point
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionLineSegments()
instead.License requirements: drafting (“DRAFTING”)
EndLocation1¶
-
HalfSectionLineBuilder.
EndLocation1
¶ Returns or sets the arrow location
-------------------------------------
Getter Method
Signature
EndLocation1
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionLineSegments()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
EndLocation1
Parameters: endLocation1 ( NXOpen.Point
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionLineSegments()
instead.License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
HalfSectionLineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.