GeneralWorkFlowBuilderSettingsOrientationType Enumeration

NXOpen.Drawings.GeneralWorkFlowBuilder.SettingsOrientationType is an alias for NXOpen.Drawings.GeneralWorkFlowBuilderSettingsOrientationType

class NXOpen.Drawings.GeneralWorkFlowBuilderSettingsOrientationType

Bases: object

Represents the settings orientation type.

Enum Members

Enum Member Enum Member Description
DrawingTemplate
DrawingStandard
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.