GeneralWorkFlowBuilderGridSettingsType Enumeration

NXOpen.Drawings.GeneralWorkFlowBuilder.GridSettingsType is an alias for NXOpen.Drawings.GeneralWorkFlowBuilderGridSettingsType

class NXOpen.Drawings.GeneralWorkFlowBuilderGridSettingsType

Bases: object

Represents the grid settings type.

Enum Members

Enum Member Enum Member Description
Drafting
Sketch
SheetZone
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.