DrawingsPropertiesBuilder Class¶
-
class
NXOpen.Drawings.
DrawingsPropertiesBuilder
¶ Bases:
NXOpen.Builder
Represents an
NXOpen.Drawings.DrawingsPropertiesBuilder
to be used for marking the component as secondary geometry.To create a new instance of this class, use
NXOpen.DraftingManager.CreateDrawingsPropertiesBuilder()
Default values.
Property Value SecondaryComponent No New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
SecondaryComponent | Returns or sets the secondary geometry state. |
SelectedObjects | Returns the selected object(s) list. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DrawingsPropertiesBuilderSecondaryComponentOptions Enumeration | Options for managing the secondary geometry property on the components |
Property Detail¶
SecondaryComponent¶
-
DrawingsPropertiesBuilder.
SecondaryComponent
¶ Returns or sets the secondary geometry state.
If true, the part occurrences are marked as secondary components. Otherwise, the part occurrences are considered as non-secondary components.
-------------------------------------
Getter Method
Signature
SecondaryComponent
Returns: Return type: NXOpen.Drawings.DrawingsPropertiesBuilderSecondaryComponentOptions
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondaryComponent
Parameters: secondaryComponent ( NXOpen.Drawings.DrawingsPropertiesBuilderSecondaryComponentOptions
) –New in version NX11.0.0.
License requirements: drafting (“DRAFTING”)
SelectedObjects¶
-
DrawingsPropertiesBuilder.
SelectedObjects
¶ Returns the selected object(s) list.
This is the active list of components that will be modified by any changes.
-------------------------------------
Getter Method
Signature
SelectedObjects
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX11.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
DrawingsPropertiesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.