DrawingSheetBuilderSheetStandardEnglishScale Enumeration¶
NXOpen.Drawings.DrawingSheetBuilder.SheetStandardEnglishScale is an alias for NXOpen.Drawings.DrawingSheetBuilderSheetStandardEnglishScale
-
class
NXOpen.Drawings.
DrawingSheetBuilderSheetStandardEnglishScale
¶ Bases:
object
the standard English drawing sheet scales
Enum Members
Enum Member Enum Member Description S81 a scale of 8:1 S41 a scale of 4:1 S21 a scale of 2:1 S11 a scale of 1:1 S12 a scale of 1:2 S14 a scale of 1:4 S18 a scale of 1:8 Custom a custom scale -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-