DrawingRegionRulesBuilder Class¶
-
class
NXOpen.Drawings.
DrawingRegionRulesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Drawing region rules builder
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
GetRules | Get Rules |
RemoveRules | Remove Rules |
SetRules | Set Rules |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetRules¶
-
DrawingRegionRulesBuilder.
GetRules
¶ Get Rules
Signature
GetRules()
Returns: Return type: list of str New in version NX8.0.0.
License requirements: None.
RemoveRules¶
-
DrawingRegionRulesBuilder.
RemoveRules
¶ Remove Rules
Signature
RemoveRules(rules)
Parameters: rules (list of str) – New in version NX8.0.0.
License requirements: nx_drawing_auto (“NX Drawing Automation”)
SetRules¶
-
DrawingRegionRulesBuilder.
SetRules
¶ Set Rules
Signature
SetRules(rules)
Parameters: rules (list of str) – New in version NX8.0.0.
License requirements: nx_drawing_auto (“NX Drawing Automation”)
Validate¶
-
DrawingRegionRulesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.