DrawingRegionBuilderContentToMove Enumeration

NXOpen.Drawings.DrawingRegionBuilder.ContentToMove is an alias for NXOpen.Drawings.DrawingRegionBuilderContentToMove

class NXOpen.Drawings.DrawingRegionBuilderContentToMove

Bases: object

Specifies the region content to move

Enum Members

Enum Member Enum Member Description
All
OnlyOverlapping
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.