DrawingCompareSettingsBuilderChangeSymbolType Enumeration

NXOpen.Drawings.DrawingCompareSettingsBuilder.ChangeSymbolType is an alias for NXOpen.Drawings.DrawingCompareSettingsBuilderChangeSymbolType

class NXOpen.Drawings.DrawingCompareSettingsBuilderChangeSymbolType

Bases: object

Represents a Compare Settings Change symbol Types

Enum Members

Enum Member Enum Member Description
Circle
TriangleUp
TriangleDown
Square
Hexagon
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.