DraftingDrawingSheetBuilder Class¶
-
class
NXOpen.Drawings.
DraftingDrawingSheetBuilder
¶ Bases:
NXOpen.Drawings.DrawingSheetBuilder
Represents a Builder for creating :py:class:`NXOpen.Drawings.DraftingDrawingSheet`s
To create a new instance of this class, use
NXOpen.Drawings.DraftingDrawingSheetCollection.CreateDraftingDrawingSheetBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
AutoStartBaseView | Returns or sets the setting that controls whether or not the Add Base View command is automatically started after inserting a sheet that has no views on it. |
AutoStartViewCreation | Returns or sets the setting that controls whether or not the Add View creation is automatically started after inserting a sheet that has no views on it. |
BaseordrawingView | Returns or sets the option of base view or drawing view |
EnglishSheetTemplateLocation | Returns or sets the location of the english drawing sheet template to be added to the part file |
Height | Returns or sets the custom or standard height for the drawing sheet |
Length | Returns or sets the custom or standard length to be used for the drawing to be created or edited. |
MetricSheetTemplateLocation | Returns or sets the location of the metric drawing sheet template to be added to the part file |
Name | Returns or sets the name of the drawing sheet to be created or edited |
Number | Returns or sets the number of the drawing sheet to be created or edited |
Option | Returns or sets the option to be used to create the drawing sheet |
ProjectionAngle | Returns or sets the projection_angle option |
Revision | Returns or sets the revision of the drawing sheet to be created or edited |
ScaleDenominator | Returns or sets the denominator of a custom scale |
ScaleNumerator | Returns or sets the numerator of a custom scale |
SecondaryNumber | Returns or sets the secondary number of the drawing sheet to be created or edited |
StandardEnglishScale | Returns or sets the standard English drawing scale |
StandardMetricScale | Returns or sets the standard Metric drawing scale |
Tag | Returns the Tag for this object. |
Units | Returns or sets the units for the drawing sheet |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Validate¶
-
DraftingDrawingSheetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.