DraftingCurveInfoDraftingCurveType Enumeration¶
NXOpen.Drawings.DraftingCurveInfo.DraftingCurveType is an alias for NXOpen.Drawings.DraftingCurveInfoDraftingCurveType
-
class
NXOpen.Drawings.
DraftingCurveInfoDraftingCurveType
¶ Bases:
object
Specifies the drafting curve types
Enum Members
Enum Member Enum Member Description ExtractedEdge Specifies Extracted Edge Curve ExtractedModelCurve Specifies Extracted Model Curve SilhouetteCurve Specifies Silhouette Curve ThreadSilhouetteCurve Specifies Thread Silhouette Curve SectionEdge Specifies Section Edge Curve ThreadSectionEdge Specifies Thread Section Edge Curve VICurve Specifies Virtual Intersection Curve UVHatchCurve Specifies UVHatch Curve TracelineCurve Specifies TraceLine Curve SimplifiedCurve Specifies Simplified Curve InterferenceCurve Specifies Interference Curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-