DraftingBodyCollection Class

class NXOpen.Drawings.DraftingBodyCollection

Bases: object

Represents a collection of :py:class:`NXOpen.Drawings.DraftingBody`s.

To obtain an instance of this class, refer to NXOpen.Drawings.DraftingView

New in version NX8.5.0.

Methods

Method Description
FindObject Finds the NXOpen.Drawings.DraftingBody with the given identifier as recorded in a journal.

Method Detail

FindObject

DraftingBodyCollection.FindObject

Finds the NXOpen.Drawings.DraftingBody with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Identifier of the DraftingBody to be found
Returns:DraftingBody with this identifier
Return type:NXOpen.Drawings.DraftingBody

New in version NX8.5.0.

License requirements: None.