CustomViewSettingsBuilderWidth Enumeration¶
NXOpen.Drawings.CustomViewSettingsBuilder.Width is an alias for NXOpen.Drawings.CustomViewSettingsBuilderWidth
-
class
NXOpen.Drawings.
CustomViewSettingsBuilderWidth
¶ Bases:
object
the width options for all the line width used in the customize view settings dialog
Enum Members
Enum Member Enum Member Description Original Original One One Two Two Three Three Four Four Five Five Six Six Seven Seven Eight Eight Nine Nine -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-