CustomViewSettingsBuilderFont Enumeration¶
NXOpen.Drawings.CustomViewSettingsBuilder.Font is an alias for NXOpen.Drawings.CustomViewSettingsBuilderFont
-
class
NXOpen.Drawings.
CustomViewSettingsBuilderFont
¶ Bases:
object
the options for all the fonts used in the custom view settings dialog
Enum Members
Enum Member Enum Member Description Invisible Invisible Solid Solid Dashed Dashed Phantom Phantom Centerline CenterLine Dotted Dotted LongDashed Long Dashed DottedDashed Dotted Dashed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-