BrokenViewBuilderBreakLineStyle Enumeration¶
NXOpen.Drawings.BrokenViewBuilder.BreakLineStyle is an alias for NXOpen.Drawings.BrokenViewBuilderBreakLineStyle
-
class
NXOpen.Drawings.
BrokenViewBuilderBreakLineStyle
¶ Bases:
object
Break Line Type
Enum Members
Enum Member Enum Member Description Simple Simple Straight Straight Sawtooth Sawtooth LongBreak LongBreak Tubular Tubular SolidTubular Solid Tubular SolidRod Solid Rod Jigsaw Jigsaw Wood Wood CopyCurve Copy of the existing curve TemplateCurve Template, based on the existing curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-