BaseViewStyle Class¶
-
class
NXOpen.Drawings.
BaseViewStyle
¶ Bases:
object
Represents set of Base View Style Preferences applicable to drafting views.
To obtain an instance of this class use
Drawings.ViewStyle.BaseView()
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
LoadModelFromPart | To load the assemblies arrangement part file. |
SetAssemblyArrangement | Sets the configuration for the arrangement in assembly after an arrangement part file is loaded. |
SetFacetedRepresentation | The status of faceted representation, if True the clipping bounds are inherited, else the imported model view is placed on the drawing with an Automatic Rectangular Boundary. |
SetInheritClippingBoundary | The status of inherit clipping boundary, if True the model view’s clipping boundary are inherited when model view is imported onto the drawing, else the imported model view is placed on the drawing with an Automatic Rectangular Boundary. |
SetTransferAnnotation | The status of transfer annotation controls whether or not annotations created in a model view are transferred to the drawing when a view is imported. |
Method Detail¶
LoadModelFromPart¶
-
BaseViewStyle.
LoadModelFromPart
¶ To load the assemblies arrangement part file.
If the logical argument is True, the part would be loaded.
Signature
LoadModelFromPart(loadPartName, loadPartToggle)
Parameters: - loadPartName (str) – name of the loaded part
- loadPartToggle (bool) – True or False status for loading the part.
New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
SetAssemblyArrangement¶
-
BaseViewStyle.
SetAssemblyArrangement
¶ Sets the configuration for the arrangement in assembly after an arrangement part file is loaded.
Signature
SetAssemblyArrangement(config)
Parameters: config (str) – name of the configuration for the arrangement New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
SetFacetedRepresentation¶
-
BaseViewStyle.
SetFacetedRepresentation
¶ The status of faceted representation, if True the clipping bounds are inherited, else the imported model view is placed on the drawing with an Automatic Rectangular Boundary.
Signature
SetFacetedRepresentation(isFacetedRepresentation)
Parameters: isFacetedRepresentation (bool) – New in version NX5.0.0.
Deprecated since version NX8.5.1: Use
Drawings.GeneralViewStyle.ViewRepresentation()
instead.License requirements: drafting (“DRAFTING”)
SetInheritClippingBoundary¶
-
BaseViewStyle.
SetInheritClippingBoundary
¶ The status of inherit clipping boundary, if True the model view’s clipping boundary are inherited when model view is imported onto the drawing, else the imported model view is placed on the drawing with an Automatic Rectangular Boundary.
Signature
SetInheritClippingBoundary(isInheritClippingBoundary)
Parameters: isInheritClippingBoundary (bool) – Inherit XY clipping boundaries of model New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
SetTransferAnnotation¶
-
BaseViewStyle.
SetTransferAnnotation
¶ The status of transfer annotation controls whether or not annotations created in a model view are transferred to the drawing when a view is imported.
Signature
SetTransferAnnotation(isTransferAnnotation)
Parameters: isTransferAnnotation (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)