NXOpen.Drafting Package

Classes

AnnotateViewsBuilder Class This class is used to annotate views based on the knowledge fusion rules.
AttributeItemBuilder Class Represents a NXOpen.Drafting.AttributeItemBuilder.
AttributeItemBuilderList Class Represents a list of objects.
AutomationManager Class Represents a NXOpen.Drafting.AutomationManager.
AutomationPreferencesBuilder Class the builder for Drafting Automation Preferences
AutomationRuleBuilder Class Represents a NXOpen.Drafting.AutomationRuleBuilder
BaseEditSettingsBuilder Class Represents a NXOpen.Drafting.BaseEditSettingsBuilder.
CutCopyPasteBuilder Class Represents a paste in Drafting.
CutCopyPasteLeaderBuilder Class Represents a Drafting Paste, especially when reassociating a leader on paste.
DistributeAnnotationsBuilder Class This class is used to distribute annotations associated to a view.
DraftingApplicationManager Class Represents an object that manages drafting objects and member views.
DrawingAutomationWizard Class Represents callback data for the drawing automation wizard.
DrawingCreationWizardBuilder Class Represents a NXOpen.Drafting.DrawingCreationWizardBuilder.
MoveToDrawingViewBuilder Class This builder allows the user to extract contents from a sheet and transfer them to a new Drawing view, also provide some other options for view creation
PreferencesBuilder Class Represents a NXOpen.Drafting.PreferencesBuilder builder
PrimaryContentItemBuilder Class Represents a NXOpen.Drafting.PrimaryContentItemBuilder.
PrimaryContentItemBuilderList Class Represents a list of objects.
RulesBuilder Class This class is used to specify knowledge fusion rules in a drawing template.
SettingsManager Class Represents an object that manages drafting settings.
SmashDrawingViewBuilder Class This builder allows the user to break a Drawing View into its parts and delete the Drawing View
SpecifyRuleBuilder Class This class is used to specify knowledge fusion rule for a note object in a drawing template.

Enumerations

AnnotateViewsBuilderExistingAutomaticAnnotation Enumeration Option to delete or preserve existing automatic annotations when annotation views command is run.
CutCopyPasteBuilderTypeOperation Enumeration Specifies the copy cut operation type.
CutCopyPasteBuilderTypePaste Enumeration Specifies the paste type.