CutCopyPasteLeaderBuilder Class¶
-
class
NXOpen.Drafting.
CutCopyPasteLeaderBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Drafting Paste, especially when reassociating a leader on paste.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
DestinationView | Returns or sets the destination view. |
IsLeaderSelection | Returns or sets the variable of is leader selection or not |
LeaderSelection | Returns the selection to reassociate single leader |
ReassociateLeader | Returns or sets the flag to reassociate a leader |
Selection | Returns the selection to reassociate leader |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
SetMoveOnCommit | Set the final motion from the drop location. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DestinationView¶
-
CutCopyPasteLeaderBuilder.
DestinationView
¶ Returns or sets the destination view.
Either a drafting view or sheet view.
-------------------------------------
Getter Method
Signature
DestinationView
Returns: Return type: NXOpen.View
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DestinationView
Parameters: destinationView ( NXOpen.View
) –New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
IsLeaderSelection¶
-
CutCopyPasteLeaderBuilder.
IsLeaderSelection
¶ Returns or sets the variable of is leader selection or not
-------------------------------------
Getter Method
Signature
IsLeaderSelection
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsLeaderSelection
Parameters: isLeaderSelection (bool) – True If it is leader selection New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
LeaderSelection¶
-
CutCopyPasteLeaderBuilder.
LeaderSelection
¶ Returns the selection to reassociate single leader
-------------------------------------
Getter Method
Signature
LeaderSelection
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX8.0.0.
License requirements: None.
ReassociateLeader¶
-
CutCopyPasteLeaderBuilder.
ReassociateLeader
¶ Returns or sets the flag to reassociate a leader
-------------------------------------
Getter Method
Signature
ReassociateLeader
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReassociateLeader
Parameters: reassociateLeader (bool) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Selection¶
-
CutCopyPasteLeaderBuilder.
Selection
¶ Returns the selection to reassociate leader
-------------------------------------
Getter Method
Signature
Selection
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX8.0.0.
License requirements: None.
Method Detail¶
SetMoveOnCommit¶
-
CutCopyPasteLeaderBuilder.
SetMoveOnCommit
¶ Set the final motion from the drop location.
Signature
SetMoveOnCommit(rot, trans)
Parameters: - rot (
NXOpen.Matrix3x3
) – rotational part of motion - trans (
NXOpen.Vector3d
) – translation part of motion
New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
- rot (
Validate¶
-
CutCopyPasteLeaderBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.