AttributeItemBuilder Class¶
-
class
NXOpen.Drafting.
AttributeItemBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Drafting.AttributeItemBuilder
.This class is used to specify information about a single NX attribute.
To create a new instance of this class, use
NXOpen.Drafting.AutomationManager.CreateAttributeItemBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Title | Returns or sets the title. |
Value | Returns or sets the value. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Title¶
-
AttributeItemBuilder.
Title
¶ Returns or sets the title.
-------------------------------------
Getter Method
Signature
Title
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Title
Parameters: attributeTitle (str) – New in version NX8.0.0.
License requirements: nx_drawing_auto (“NX Drawing Automation”)
Value¶
-
AttributeItemBuilder.
Value
¶ Returns or sets the value.
-------------------------------------
Getter Method
Signature
Value
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value
Parameters: attributeValue (str) – New in version NX8.0.0.
License requirements: nx_drawing_auto (“NX Drawing Automation”)
Method Detail¶
Validate¶
-
AttributeItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.