AnnotateViewsBuilderExistingAutomaticAnnotation Enumeration

NXOpen.Drafting.AnnotateViewsBuilder.ExistingAutomaticAnnotation is an alias for NXOpen.Drafting.AnnotateViewsBuilderExistingAutomaticAnnotation

class NXOpen.Drafting.AnnotateViewsBuilderExistingAutomaticAnnotation

Bases: object

Option to delete or preserve existing automatic annotations when annotation views command is run.

Enum Members

Enum Member Enum Member Description
Delete
Preserve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.