DisplayPartOption Enumeration¶
-
class
NXOpen.
DisplayPartOption
¶ Bases:
object
Controls whether or not a new display part may be displayed in addition to existing display parts, or instead of the currently active display part. See
NXOpen.PartCollection.SetActiveDisplay()
New in version NX12.0.0.
Enum Members
Enum Member Enum Member Description ReplaceExisting Replace the existing active display part with the new one AllowAdditional If possible display the new part as an additional display part -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-