BackgroundBackgroundDomeType Enumeration |
dome types |
BackgroundCategoryType Enumeration |
background 2D3D types |
BackgroundType Enumeration |
background types |
BoundedGridBuilderLabelReferenceType Enumeration |
Specifies label reference. |
BoundedGridBuilderShowLabelType Enumeration |
Specifies label option to be used for grid label display. |
CameraBuilderAperture Enumeration |
Predefined apertures: f2. |
CameraBuilderFovMeasured Enumeration |
either horizontal or vertical measure |
CameraBuilderLensAngle Enumeration |
the way to define the field of view angle |
CameraBuilderLensFlare Enumeration |
Predefined lens flare types: Standard, 35mm, 50mm, 105mm, polygonal, 35mm poly, 50mm poly, 105mm poly, spark, star |
CameraBuilderStockLens Enumeration |
Predefined lenses: 28, 35, 50, 70, 105, 135, 210, 300mm |
CameraBuilderTypes Enumeration |
the camera types |
CanonMRTestBuilderImageUsageType Enumeration |
Indicates how the image identified by ImageFile is specified to CGP. |
DatumPlaneGridBuilderGridOrientationType Enumeration |
Specifies grid orientation option to be used for grid display. |
DecalBuilderAnchor Enumeration |
image anchor |
DecalBuilderDecalIllumination Enumeration |
decal illumination type |
DecalBuilderDecalReflectivities Enumeration |
decal reflectivity type |
DecalBuilderImageSize Enumeration |
image size type |
DecalBuilderScaling Enumeration |
decal scaling type |
DynamicSectionTypesActivePlane Enumeration |
Specifies active clip plane in the active plane pair. |
DynamicSectionTypesAxis Enumeration |
Specifies axis. |
DynamicSectionTypesCapColorOption Enumeration |
Specifies cap color type to be used for the cap. |
DynamicSectionTypesClip Enumeration |
Specifies clipping type. |
DynamicSectionTypesCoordinateSystem Enumeration |
Specifies the coordinate system used for creating principal planes i. |
DynamicSectionTypesCurveColorOption Enumeration |
Specifies the color of the curves created by the section plane. |
DynamicSectionTypesType Enumeration |
Specifies different type of sectioning. |
EnvironmentBuilderGroundPlaneTypes Enumeration |
Represents an index to a ground plane type define |
EnvironmentBuilderImageBlurType Enumeration |
lighting image blurr type |
EnvironmentBuilderImageUpVectorTypes Enumeration |
up vector type |
EnvironmentBuilderToneMappingTypes Enumeration |
tone mapping type - do not enable until NX11 |
FacetSettingsBuilderAdvVisToleranceSetting Enumeration |
Specifies which set of tolerances are to be used for rendering facets for display for Advanced Visualization views. |
FacetSettingsBuilderFacetScale Enumeration |
Denotes what type of scaling factor is applied to the corresponding tolerances used to generate facets. |
FacetSettingsBuilderFacetToViewRatio Enumeration |
Specifies whether the ratio of the view scale to the scale used to generate facets is determined automatically by the system (as was always done before NX 8) or whether a ratio defined by the user (by one of the set_*FacetRatio methods) is to be used as the ratio. |
FacetSettingsBuilderFacetUpdate Enumeration |
Specifies whether an Update Display or Fit operation is to regenerate the facets for only visible objects, for all objects or for no objects. |
FacetSettingsBuilderShadedToleranceSetting Enumeration |
Specifies which set of tolerances are to be used for rendering facets for display for Shaded views. |
GridBuilderLineStyleType Enumeration |
Specifies line style to be used for major and minor lines of the grid. |
GridBuilderLineWeightType Enumeration |
Specifies line weight to be used for major and minor lines of the grid. |
IRayPlusStudioEditorBuilderDynamicIRayPlusStudioRenderModeType Enumeration |
To specify the quality and performance of the Ray Traced Studio display when dynamic interaction stops |
IRayPlusStudioEditorBuilderIRayPlusStudioRemoteRenderFormatType Enumeration |
To specify the Ray Traced Studio remote rendering format |
IRayPlusStudioEditorBuilderIRayPlusStudioRemoteRenderType Enumeration |
To specify the Ray Traced Studio remote rendering type |
IRayPlusStudioEditorBuilderIRayPlusStudioRemoteRenderVideoType Enumeration |
To specify the Ray Traced Studio remote rendering video mode |
IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageFileFormatType Enumeration |
To specify the Ray Traced Studio static image file format |
IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageOrientationType Enumeration |
To specify the Ray Traced Studio static image orientation |
IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageResolutionType Enumeration |
To specify the Ray Traced Studio static image resolution |
IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageSizeType Enumeration |
To specify the Ray Traced Studio static image size |
IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageUnitsType Enumeration |
To specify the Ray Traced Studio static image units |
ImageBaseBuilderBasePointChoices Enumeration |
Specifies image reference base point choice. |
ImageBaseBuilderImageColorModes Enumeration |
Describes image color modes. |
ImageBaseBuilderInsertionPoint Enumeration |
Describes insertion point type. |
ImageBaseBuilderReferenceDirection Enumeration |
Specifies image alignment reference direction type. |
ImageBaseBuilderSizeOptions Enumeration |
Describes size options. |
ImageBaseBuilderTransparencyColorFrom Enumeration |
Transparency Color From |
ImageBasedLightingImageBlurType Enumeration |
lighting image blurr type |
ImageBasedLightingImageUpVectorTypes Enumeration |
up vector type |
ImageBasedLightingImagesType Enumeration |
images type - environment used for generating image-based lighting |
ImageBasedLightingShadowsType Enumeration |
shadow type |
IrayPlusMaterialEditorBuilderLayerType Enumeration |
Layer types used in iray plus material |
IrayPlusSimpleMaterialEditorBuilderTextureSpace Enumeration |
texture spacee type |
LayerSettingsBuilderLayerOptionType Enumeration |
Specifies the layer options. |
LightBuilderLightMode Enumeration |
light_mode |
LightBuilderShadowType Enumeration |
shadow types |
NonProportionalZoomMethodType Enumeration |
Sets the kind of mouse interaction that will define the non-proportional zoom. |
PlanarShipGridBuilderIntersectOption Enumeration |
Settings that indicate how to search for objects that intersect the plane. |
PlanarShipGridBuilderLabelDisplayOption Enumeration |
Settings that indicate what grid lines should be labelled. |
PointCloudBuilderBrightnessModes Enumeration |
Specifies point cloud brightness display mode choice. |
PointCloudBuilderColorModes Enumeration |
Specifies point cloud color display mode choice. |
PointCloudClippingBoxesListItemBuilderClippingSides Enumeration |
Specifies clipping side options used for defined clipping box. |
RayTracedStudioBuilderStationaryDisplayQualityType Enumeration |
To specify the quality and performance of the Ray Traced Studio display. |
RayTracedStudioEditorBuilderDynamicRayTracedStudioTilingQualityType Enumeration |
To specify the quality and performance of the interactive, dynamic Ray Traced Studio display. |
RayTracedStudioEditorBuilderRayTracedStudioStaticImageFileFormatType Enumeration |
To specify the Ray Traced Studio static image file format |
RayTracedStudioEditorBuilderRayTracedStudioStaticImageOrientationType Enumeration |
To specify the Ray Traced Studio static image orientation |
RayTracedStudioEditorBuilderRayTracedStudioStaticImageResolutionType Enumeration |
To specify the Ray Traced Studio static image resolution |
RayTracedStudioEditorBuilderRayTracedStudioStaticImageSizeType Enumeration |
To specify the Ray Traced Studio static image size |
RayTracedStudioEditorBuilderRayTracedStudioStaticImageUnitsType Enumeration |
To specify the Ray Traced Studio static image units |
RayTracedStudioEditorBuilderStaticAntialiasingType Enumeration |
To specify the antialiasing quality during stationary Ray Traced Studio display during static image rendering |
RayTracedStudioEditorBuilderStaticRayTracedStudioQualityType Enumeration |
To specify the quality and performance of the Ray Traced Studio display during static image rendering |
RayTracedStudioEditorBuilderStationaryAntialiasingType Enumeration |
To specify the antialiasing quality during stationary Ray Traced Studio display when dynamic interaction stops |
RayTracedStudioEditorBuilderStationaryRayTracedStudioQualityType Enumeration |
To specify the quality and performance of the Ray Traced Studio display when dynamic interaction stops |
ReflectionType Enumeration |
where the reflections for rendering will be obtained |
SaveImageFileBrowserBuilderFileFormats Enumeration |
To specify the Ray Traced Studio static image file format |
SectionCurveSettingsBuilderColorOptionType Enumeration |
Specifies the color of the curves. |
SelPrefFaceAnalysisViews Enumeration |
Represents the face analysis views type |
SelPrefMethod Enumeration |
Represents the chaining method type |
SelPrefMouseGesture Enumeration |
Represents the mouse gesture type |
SelPrefSelectionRadius Enumeration |
Represents the selection radius type |
SelPrefSelectionRule Enumeration |
Represents the selection rule type |
SelPrefShadedViews Enumeration |
Represents the shaded views type |
SelectFontFileBuilderFontCyclingType Enumeration |
Specifies whether available fonts are automatically cycled. |
SelectFontFileBuilderGeometryType Enumeration |
Specifies the coordinate spaces of text geometry. |
SelectFontFileBuilderHiddenStyleType Enumeration |
Specifies the behavior of hidden text. |
SelectFontFileBuilderJustificationType Enumeration |
Specifies how glyphs are justified in the text box. |
SelectFontFileBuilderLayoutType Enumeration |
Identifies the text layout, which defines the direction in which glyphs advance or flow along a single line, and the direction in which lines advance or flow along a page. |
SelectFontFileBuilderRefLocation Enumeration |
Identifies the location on the text box used to position text. |
SelectFontFileBuilderRotation2dType Enumeration |
Specifies how Screen text is rotated in the plane of the screen. |
ShadowsRealTimeState Enumeration |
Real time type settings - environment_shadow_catcher_only is enabled only in Basic Studio mode |
ShadowsSsaoContrastType Enumeration |
Shadows SSAO contrast settings |
ShadowsSsaoQualityType Enumeration |
Shadows SSAO quality settings |
StageOrientationType Enumeration |
Represents an index to a floor plane type define |
StageWallType Enumeration |
Represents an index to a particular wall in the stage. |
StudioImageCaptureBuilderAASamplesEnumType Enumeration |
Provide the following anti-aliasing sample size for off screen image capture |
StudioImageCaptureBuilderDPIEnumType Enumeration |
Provide the following screen capture resolutions in dots per inch |
StudioImageCaptureBuilderDrawingSizeEnumType Enumeration |
Provide the following standard Drawing sizes |
StudioImageCaptureBuilderOrientEnumType Enumeration |
Provide the following options to image orientation |
StudioImageCaptureBuilderUnitsEnumType Enumeration |
Provide the following resolution unit options to screen capture |
TransientTextStandardTextRef Enumeration |
This enumerated type specifies the type of reference point used in the text box for standard_text methods. |
TransientTextTextSize Enumeration |
Provides a way to specify the size of the desired text, as small, medium or large (normal is a synonym for medium). |
TransientTextViewType Enumeration |
the view or views in which the transient text is to be displayed. |
TrueShadingBuilderBgdImageType Enumeration |
Background image types |
TrueShadingBuilderBgdType Enumeration |
Background colors and image types |
TrueShadingBuilderEnvironmentMapType Enumeration |
Global environment reflection map types |
TrueShadingBuilderMaterialType Enumeration |
Global material and per object overriding material types |
TrueShadingBuilderSHEDLightCollectionType Enumeration |
Scene lighting collection types |
TrueShadingBuilderSurfaceOrientType Enumeration |
Shadow plane projection orientation types |
TrueStudioBuilderGlobalMaterial Enumeration |
Types of True Studio Global Material display. |
TrueStudioBuilderRenderMethod Enumeration |
Types of True Studio Render Methods. |
WallMaterialTextureType Enumeration |
the new wall material texture type |
WallMaterialType Enumeration |
Defines the material characteristics of a stage wall. |