TrueStudioCollection Class

class NXOpen.Display.TrueStudioCollection

Bases: object

Represents a collection TrueStudio objects

To obtain an instance of this class, refer to NXOpen.BasePart

New in version NX6.0.0.

Methods

Method Description
CreateTrueStudioBuilder Creates a NXOpen.Display.TrueStudioBuilder object if TrueStudio is None.
FindObject Finds the NXOpen.Display.TrueStudio with the given identifier as recorded in a journal.

Method Detail

CreateTrueStudioBuilder

TrueStudioCollection.CreateTrueStudioBuilder

Creates a NXOpen.Display.TrueStudioBuilder object if TrueStudio is None.

Otherwise, a TrueStudio object will be edited

Signature CreateTrueStudioBuilder(sObj)

Parameters:sObj (NXOpen.Display.TrueStudio) – If TrueStudio object is not None, then this object will be edited
Returns:return TrueStudio object builder
Return type:NXOpen.Display.TrueStudioBuilder

New in version NX6.0.0.

License requirements: None.

FindObject

TrueStudioCollection.FindObject

Finds the NXOpen.Display.TrueStudio with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Identifier to be found
Returns:TrueStudio object found
Return type:NXOpen.Display.TrueStudio

New in version NX6.0.0.

License requirements: None.