TrueStudioBuilderRenderMethod Enumeration¶
NXOpen.Display.TrueStudioBuilder.RenderMethod is an alias for NXOpen.Display.TrueStudioBuilderRenderMethod
-
class
NXOpen.Display.
TrueStudioBuilderRenderMethod
¶ Bases:
object
Types of True Studio Render Methods. The render method is used to specify display quality or real-time performance
Enum Members
Enum Member Enum Member Description FullRender All rendering effects are honored. ImprovedRender Some rendering effects are not honored. Can be faster than Full Render. PreviewRender Many rendering effects are not honored. Faster than Full and Improved Render. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-