TrueShadingBuilderEnvironmentMapType Enumeration¶
NXOpen.Display.TrueShadingBuilder.EnvironmentMapType is an alias for NXOpen.Display.TrueShadingBuilderEnvironmentMapType
-
class
NXOpen.Display.
TrueShadingBuilderEnvironmentMapType
¶ Bases:
object
Global environment reflection map types
Enum Members
Enum Member Enum Member Description Default No reflection map MetalShiny1 Shiny Metal Reflection 1 MetalShiny2 Shiny Metal Reflection 2 MetalBrushed1 Brushed Metal Reflection 1 MetalBrushed2 Brushed Metal Reflection 2 Glossy1 Glossy Reflection 1 Glossy2 Glossy Reflection 2 SurfaceAnalysisLines Surface Analysis Lines Reflection SurfaceAnalysisHorizon Surface Analysis Horizontal Lines Reflection AutoPhotoStudio Automotive Lighting Reflection CustomImage Custom Image Reflection -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-