TrueShadingBuilderBgdImageType Enumeration¶
NXOpen.Display.TrueShadingBuilder.BgdImageType is an alias for NXOpen.Display.TrueShadingBuilderBgdImageType
-
class
NXOpen.Display.
TrueShadingBuilderBgdImageType
¶ Bases:
object
Background image types
Enum Members
Enum Member Enum Member Description Image1 Predefined image 1 background Image2 Predefined image 2 background Image3 Predefined image 3 background Image4 Predefined image 4 background Image5 Predefined image 5 background Image6 Predefined image 6 background CustomImage Custom image background -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-