TransientTextTextSize Enumeration¶
NXOpen.Display.TransientText.TextSize is an alias for NXOpen.Display.TransientTextTextSize
-
class
NXOpen.Display.
TransientTextTextSize
¶ Bases:
object
Provides a way to specify the size of the desired text, as small, medium or large (normal is a synonym for medium).
Enum Members
Enum Member Enum Member Description Small Normal Medium Large NumSizes -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-