TransientTextStandardTextRef Enumeration¶
NXOpen.Display.TransientText.StandardTextRef is an alias for NXOpen.Display.TransientTextStandardTextRef
-
class
NXOpen.Display.
TransientTextStandardTextRef
¶ Bases:
object
This enumerated type specifies the type of reference point used in the text box for standard_text methods.
Enum Members
Enum Member Enum Member Description SystemDefault Display the text using the system default reference point position BaselineStart Display the text starting on the baseline, at the left end of the text box for left-to-right text, or at the right end of the text box for right-to-left text BaselineCenter Display the text with the given position in the horizontal center of the text box at the baseline BaselineEnd Display the text starting on the baseline, at the right end of the text box for left-to-right text, or at the left end of the text box for right-to-left text TopLeft Display the text with the given position in the top left of the text box TopCenter Display the text with the given position in the top center of the text box TopRight Display the text with the given position in the top right of the text box MiddleLeft Display the text with the given position in the middle left of the text box MiddleCenter Display the text with the given position in middle center of text box MiddleRight Display the text with the given position in middle right of text box BottomLeft Display the text with the given position in bottom left of text box BottomCenter Display the text with the given position in bottom center of text box BottomRight Display the text with the given position in bottom right of text box -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-