StudioImageCaptureBuilderDPIEnumType Enumeration¶
NXOpen.Display.StudioImageCaptureBuilder.DPIEnumType is an alias for NXOpen.Display.StudioImageCaptureBuilderDPIEnumType
-
class
NXOpen.Display.
StudioImageCaptureBuilderDPIEnumType
¶ Bases:
object
Provide the following screen capture resolutions in dots per inch
Enum Members
Enum Member Enum Member Description Dpi72 Set image at 72 DPI resolution Dpi150 Set image at 150 DPI resolution -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-