StudioImageCaptureBuilderAASamplesEnumType Enumeration¶
NXOpen.Display.StudioImageCaptureBuilder.AASamplesEnumType is an alias for NXOpen.Display.StudioImageCaptureBuilderAASamplesEnumType
-
class
NXOpen.Display.
StudioImageCaptureBuilderAASamplesEnumType
¶ Bases:
object
Provide the following anti-aliasing sample size for off screen image capture
Enum Members
Enum Member Enum Member Description Sam0X Do not set sampling option Sam2X Set sampling at 2 times Sam4X Set sampling at 4 times Sam8X Set sampling at 8 times Sam16X Set sampling at 16 times -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-