StageOrientationType Enumeration¶
NXOpen.Display.Stage.OrientationType is an alias for NXOpen.Display.StageOrientationType
-
class
NXOpen.Display.
StageOrientationType
¶ Bases:
object
Represents an index to a floor plane type define
Enum Members
Enum Member Enum Member Description Yz Use yz plane for the stage floor. Xz Use xz plane for the stage floor. Xy Use xy plane for the stage floor. UserDefined Use user defined plane for the stage floor. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-