SelectFontFileBuilderLayoutType Enumeration¶
NXOpen.Display.SelectFontFileBuilder.LayoutType is an alias for NXOpen.Display.SelectFontFileBuilderLayoutType
-
class
NXOpen.Display.
SelectFontFileBuilderLayoutType
¶ Bases:
object
Identifies the text layout, which defines the direction in which glyphs advance or flow along a single line, and the direction in which lines advance or flow along a page.
Enum Members
Enum Member Enum Member Description LeftToRight A horizontal layout in which the direction of glyph flow on each line is from left-to-right, and the direction of line flow is from top-to-bottom. RightToLeft A horizontal layout in which the direction of glyph flow on each line is from right-to-left, and the direction of line flow is from top-to-bottom (e.g. Hebrew). TopToBottom A vertical layout in which the direction of glyph flow on each line is from top-to-bottom, and the direction of line flow is from right-to-left (e.g. Chinese, Japanese, Korean). -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-