SelectFontFileBuilderFontCyclingType Enumeration¶
NXOpen.Display.SelectFontFileBuilder.FontCyclingType is an alias for NXOpen.Display.SelectFontFileBuilderFontCyclingType
-
class
NXOpen.Display.
SelectFontFileBuilderFontCyclingType
¶ Bases:
object
Specifies whether available fonts are automatically cycled.
Enum Members
Enum Member Enum Member Description Off On Continuous -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-