SelPrefMethod Enumeration¶
NXOpen.Display.SelPref.Method is an alias for NXOpen.Display.SelPrefMethod
-
class
NXOpen.Display.
SelPrefMethod
¶ Bases:
object
Represents the chaining method type
Enum Members
Enum Member Enum Member Description Simple chaining method simple Wcs chaining method wcs WcsLeft chaining method wcs left WcsRight chaining method wcs right -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-