RayTracedStudioEditorBuilderStationaryAntialiasingType Enumeration¶
NXOpen.Display.RayTracedStudioEditorBuilder.StationaryAntialiasingType is an alias for NXOpen.Display.RayTracedStudioEditorBuilderStationaryAntialiasingType
-
class
NXOpen.Display.
RayTracedStudioEditorBuilderStationaryAntialiasingType
¶ Bases:
object
To specify the antialiasing quality during stationary Ray Traced Studio display when dynamic interaction stops
Enum Members
Enum Member Enum Member Description Medium Good antialiasing performed when dynamic interaction stops Low Coarse antialiasing performed when dynamic interaction stops NotSet No antialiasing performed to provide quick, preview of ray traced display when dynamic interaction stops -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-