NonProportionalZoomMethodType Enumeration¶
NXOpen.Display.NonProportionalZoom.MethodType is an alias for NXOpen.Display.NonProportionalZoomMethodType
-
class
NXOpen.Display.
NonProportionalZoomMethodType
¶ Bases:
object
Sets the kind of mouse interaction that will define the non-proportional zoom.
Enum Members
Enum Member Enum Member Description Rectangle Uses a rectangular region to be zoomed. Dynamic Defines a line to define aspect ratio of non-proportional zoom. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-