LightBuilderShadowType Enumeration¶
NXOpen.Display.LightBuilder.ShadowType is an alias for NXOpen.Display.LightBuilderShadowType
-
class
NXOpen.Display.
LightBuilderShadowType
¶ Bases:
object
shadow types
Enum Members
Enum Member Enum Member Description NotSet No shadows will be produced. SoftEdged Soft-edged,approximated shadows will be generated using a shadow mapping algorithm. HardEdged Hard-edged, precise shadows will be generated using a ray-tracing algorithm. TranslucentHard Hard-edged, precise shadows will be generated using a ray-tracing algorithm. Shadows from translucent objects will also be generated and their color will be determined by the transparent object’s color. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-