IrayPlusMaterialEditorBuilderLayerType Enumeration¶
NXOpen.Display.IrayPlusMaterialEditorBuilder.LayerType is an alias for NXOpen.Display.IrayPlusMaterialEditorBuilderLayerType
-
class
NXOpen.Display.
IrayPlusMaterialEditorBuilderLayerType
¶ Bases:
object
Layer types used in iray plus material
Enum Members
Enum Member Enum Member Description Coatings Coating layers Base Base layer Geometry Base Geometry layer TextureSpace Global texture space layer MaxNumber max layer type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-